Increase the capabilities of your Raspberry Pi
with our extensive range of accessories

Raspberry Pi

Buy your Raspberry Pi today from RS Components

The Raspberry Pi is a small, powerful and lightweight ARM based computer which can do many of the things a desktop PC can do. The powerful graphics capabilities and HDMi video output make it ideal for multimedia applications such as media centres and narrowcasting solutions. The Raspberry Pi is based on a Broadcom BCM2835 chip. It does not feature a built-in hard disk or solid-state drive, instead relying on an SD card for booting and long-term storage.

So whether you want to learn to programme, hack around with some hardware or design it in at the core of your innovative new device. The only challenge is deciding what you will do with yours?

Personal use
Business use
New IR Camera from Raspberry Pi

New IR Camera from Raspberry Pi

Pi NoIR is the new high definition infrared camera module from Raspberry Pi. The IR camera features the same 5 megapixel image sensor as the standard visible light camera with the optical light filter removed to enable IR light frequencies. Compatible with Raspberry Pi model A & model B, the sensor is capable of taking still photos with a resolution of 2592x1944 and can record up to 1080p HD videos at 30 frames per second. More...

The extended spectral range of the Pi NoIR means that it can be used in a range interesting applications including infragrams (monitoring plant health), astrophotography and nocturnal wildlife photography.

Raspberry Pi

Raspberry Pi Accessories

Raspberry Pi frequently asked questions

How do I get my Raspberry Pi Camera Module up and running?

Firstly make sure that the SD card being used contains the latest Debian Raspberry Pi operating system. To check this, visit Raspberry Pi Downloads where the latest version is listed and available for download. For further instructions on how to upload the latest operating system, please visit DesignSpark.com.

Secondly, connect the Raspberry Pi Camera Module to the Raspberry Pi Board by inserting the flex cable in to the connector situated between the Ethernet and HDMI ports with the silver connectors facing the HDMI port. For further information please view the dedicated video at YouTube for a demonstration on how to do this.

Lastly, boot the Raspberry Pi up, log in and start using the Raspberry Pi Camera software. For further information and guidance on this please visit DesignSpark.com.

© RS Components Ltd Suite 1601, Level 16, Tower 1, Kowloon Commerce Centre, 51 Kwai Cheong Road, Kwai Chung, Hong Kong
RS Web Helpline: (852) 2421 9898 or Email: onlinehelp.hk@rs-components.com (9:00am-6:00pm Monday - Friday)